Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static RoutingPath.ContinueUpdOnError |
RoutingPath.ContinueUpdOnError.FALSE |
static RoutingPath.ContinueUpdOnError |
RoutingPath.ContinueUpdOnError.TRUE |
Modifier and Type | Method and Description |
---|---|
RoutingPath.ContinueUpdOnError |
RoutingPath.getContinueUpdateOnError()
Query default down direction for fixed length splines
License requirements: routing_base ("Routing Basic") . |
static RoutingPath.ContinueUpdOnError |
RoutingPath.ContinueUpdOnError.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RoutingPath.ContinueUpdOnError |
RoutingPath.ContinueUpdOnError.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RoutingPath.ContinueUpdOnError[] |
RoutingPath.ContinueUpdOnError.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RoutingPath.setContinueUpdateOnError(RoutingPath.ContinueUpdOnError update)
License requirements: routing_base ("Routing Basic") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.