Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
RoutingPartLibrary.ColumnStatus |
RoutingPartLibrary.Column.hidden
Whether or not the column is used for selection
in the specify item dialog.
|
static RoutingPartLibrary.ColumnStatus |
RoutingPartLibrary.ColumnStatus.HIDDEN
Column is not displayed in Specify Item.
|
static RoutingPartLibrary.ColumnStatus |
RoutingPartLibrary.ColumnStatus.NOT_HIDDEN
Column is displayed in Specify Item.
|
Modifier and Type | Method and Description |
---|---|
static RoutingPartLibrary.ColumnStatus |
RoutingPartLibrary.ColumnStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RoutingPartLibrary.ColumnStatus |
RoutingPartLibrary.ColumnStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RoutingPartLibrary.ColumnStatus[] |
RoutingPartLibrary.ColumnStatus.values()
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
Column(String nameInitial,
RoutingPartLibrary.ColumnStatus hiddenInitial,
RoutingPartLibrary.ColumnType typeInitial)
Constructor for the Column object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.