Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static PartVisualizationShade.ShadedViewToleranceType |
PartVisualizationShade.ShadedViewToleranceType.COARSE
For Coarse: Facet Edge Tolerance is 0.01, Facet
Chord Tolerance is 0.01, and Angular Tolerance is 0.0
|
static PartVisualizationShade.ShadedViewToleranceType |
PartVisualizationShade.ShadedViewToleranceType.CUSTOMIZE
Customize.
|
static PartVisualizationShade.ShadedViewToleranceType |
PartVisualizationShade.ShadedViewToleranceType.EXTRAFINE
For Extrafine: Facet Edge Tolerance is 0.005, Facet
Chord Tolerance is 0.001, and Angular Tolerance is 6
|
static PartVisualizationShade.ShadedViewToleranceType |
PartVisualizationShade.ShadedViewToleranceType.FINE
For Fine: Facet Edge Tolerance is 0.0005, Facet
Chord Tolerance is 0.0025, and Angular Tolerance is 6
|
static PartVisualizationShade.ShadedViewToleranceType |
PartVisualizationShade.ShadedViewToleranceType.STANDARD
For Standard: Facet Edge Tolerance is 0.005, Facet
Chord Tolerance is 0.005 , and Angular Tolerance is 15
|
static PartVisualizationShade.ShadedViewToleranceType |
PartVisualizationShade.ShadedViewToleranceType.ULTRAFINE
For Ultrafine: Facet Edge Tolerance is 0.0005, Facet
Chord Tolerance is 0.0005, and Angular Tolerance is 3
|
Modifier and Type | Method and Description |
---|---|
PartVisualizationShade.ShadedViewToleranceType |
PartVisualizationShade.shadedViewTolerance()
Returns the tolerance for shaded views.
|
static PartVisualizationShade.ShadedViewToleranceType |
PartVisualizationShade.ShadedViewToleranceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartVisualizationShade.ShadedViewToleranceType |
PartVisualizationShade.ShadedViewToleranceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartVisualizationShade.ShadedViewToleranceType[] |
PartVisualizationShade.ShadedViewToleranceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
PartVisualizationShade.ShadedViewFacetTolerancesData |
PartVisualizationShade.getShadedViewFacetTolerances(PartVisualizationShade.ShadedViewToleranceType shadedViewToleranceSet)
Returns the edge, face and angle tolerances to be used with the specified
tolerance set for shaded views.
|
void |
PartVisualizationShade.setShadedViewFacetTolerances(PartVisualizationShade.ShadedViewToleranceType shadedViewToleranceSet,
double edgeTolerance,
double faceTolerance,
double angleTolerance)
Sets the edge, face and angle tolerances to be used with the specified
tolerance set for shaded views.
|
void |
PartVisualizationShade.setShadedViewTolerance(PartVisualizationShade.ShadedViewToleranceType shadedViewTolerance)
Sets the tolerance for shaded views.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.