Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static PartVisualizationShade.HiddenShadedFaceEdges |
PartVisualizationShade.HiddenShadedFaceEdges.DASHED
If selected, hidden shaded face edges are
displayed in the body color with a dashed line
font.
|
static PartVisualizationShade.HiddenShadedFaceEdges |
PartVisualizationShade.HiddenShadedFaceEdges.HIDDEN_COLOR
If any color is selected, hidden shaded face
edges are displayed in that color.
|
static PartVisualizationShade.HiddenShadedFaceEdges |
PartVisualizationShade.HiddenShadedFaceEdges.INVISIBLE
If selected, shaded face edges that are
hidden are not displayed
|
Modifier and Type | Method and Description |
---|---|
static PartVisualizationShade.HiddenShadedFaceEdges |
PartVisualizationShade.HiddenShadedFaceEdges.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartVisualizationShade.HiddenShadedFaceEdges |
PartVisualizationShade.HiddenShadedFaceEdges.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartVisualizationShade.HiddenShadedFaceEdges[] |
PartVisualizationShade.HiddenShadedFaceEdges.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.