Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Method and Description |
---|---|
PartVisualizationShade.AdvViewToleranceType |
DisplayResolutionBuilder.resolution()
Returns the resolution
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
DisplayResolutionBuilder.setResolution(PartVisualizationShade.AdvViewToleranceType resolution)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Modifier and Type | Field and Description |
---|---|
static PartVisualizationShade.AdvViewToleranceType |
PartVisualizationShade.AdvViewToleranceType.COARSE
Coarse
|
static PartVisualizationShade.AdvViewToleranceType |
PartVisualizationShade.AdvViewToleranceType.CUSTOMIZE
Customize.
|
static PartVisualizationShade.AdvViewToleranceType |
PartVisualizationShade.AdvViewToleranceType.EXTRAFINE
Extrafine
|
static PartVisualizationShade.AdvViewToleranceType |
PartVisualizationShade.AdvViewToleranceType.FINE
Fine
|
static PartVisualizationShade.AdvViewToleranceType |
PartVisualizationShade.AdvViewToleranceType.STANDARD
Standard
|
static PartVisualizationShade.AdvViewToleranceType |
PartVisualizationShade.AdvViewToleranceType.SUPERFINE
Superfine
|
static PartVisualizationShade.AdvViewToleranceType |
PartVisualizationShade.AdvViewToleranceType.ULTRAFINE
Ultrafine
|
Modifier and Type | Method and Description |
---|---|
PartVisualizationShade.AdvViewToleranceType |
PartVisualizationShade.advancedVisViewTolerance()
Returns the tolerance for advanced visualization views.
|
static PartVisualizationShade.AdvViewToleranceType |
PartVisualizationShade.AdvViewToleranceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartVisualizationShade.AdvViewToleranceType |
PartVisualizationShade.AdvViewToleranceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartVisualizationShade.AdvViewToleranceType[] |
PartVisualizationShade.AdvViewToleranceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
PartVisualizationShade.AdvVisViewFacetTolerancesData |
PartVisualizationShade.getAdvVisViewFacetTolerances(PartVisualizationShade.AdvViewToleranceType advVisViewToleranceSet)
Returns the edge, face, angle and width tolerances to be used with the specified
tolerance set for Advanced Visualization views.
|
void |
PartVisualizationShade.setAdvancedVisViewTolerance(PartVisualizationShade.AdvViewToleranceType advancedVisViewTolerance)
Sets the tolerance for advanced visualization views.
|
void |
PartVisualizationShade.setAdvVisViewFacetTolerances(PartVisualizationShade.AdvViewToleranceType advVisViewToleranceSet,
double edgeTolerance,
double faceTolerance,
double angleTolerance,
double widthTolerance)
Sets the edge, face, angle and width tolerances to be used with the specified
tolerance set for Advanced Visualization views.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.