Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static PartDrafting.UpdateViewWithoutLwDataOption |
PartDrafting.UpdateViewWithoutLwDataOption.DO_NOT_NOTIFY
Do Not Notify
|
static PartDrafting.UpdateViewWithoutLwDataOption |
PartDrafting.UpdateViewWithoutLwDataOption.GENERATE
Generate
|
static PartDrafting.UpdateViewWithoutLwDataOption |
PartDrafting.UpdateViewWithoutLwDataOption.IGNORE
Ignore
|
static PartDrafting.UpdateViewWithoutLwDataOption |
PartDrafting.UpdateViewWithoutLwDataOption.NOTIFY
Notify
|
Modifier and Type | Method and Description |
---|---|
PartDrafting.UpdateViewWithoutLwDataOption |
PartDrafting.updateViewWithoutLwData()
Returns the option specifying the action when missing, incomplete or invalid lightweight
bodies are found during view create or update
License requirements: None. |
static PartDrafting.UpdateViewWithoutLwDataOption |
PartDrafting.UpdateViewWithoutLwDataOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartDrafting.UpdateViewWithoutLwDataOption |
PartDrafting.UpdateViewWithoutLwDataOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartDrafting.UpdateViewWithoutLwDataOption[] |
PartDrafting.UpdateViewWithoutLwDataOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PartDrafting.setUpdateViewWithoutLwData(PartDrafting.UpdateViewWithoutLwDataOption updateViewWithoutLWDataOption)
Sets the option specifying the action when missing, incomplete or invalid lightweight
bodies are found during view create or update
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.