public static class SessionModeling.ImmediateChildrenType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALL
Indicates that Immediate Children type is at all level
|
static int |
_FIRST_LEVEL
Indicates that Immediate Children type is at first level
|
static SessionModeling.ImmediateChildrenType |
ALL
Indicates that Immediate Children type is at all level
|
static SessionModeling.ImmediateChildrenType |
FIRST_LEVEL
Indicates that Immediate Children type is at first level
|
Modifier and Type | Method and Description |
---|---|
static SessionModeling.ImmediateChildrenType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionModeling.ImmediateChildrenType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionModeling.ImmediateChildrenType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SessionModeling.ImmediateChildrenType FIRST_LEVEL
public static final SessionModeling.ImmediateChildrenType ALL
public static final int _FIRST_LEVEL
public static final int _ALL
public static SessionModeling.ImmediateChildrenType valueOf(int value)
public static SessionModeling.ImmediateChildrenType valueOf(String name)
public static SessionModeling.ImmediateChildrenType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.