public static class SessionModeling.DynamicUpdateType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CONTINUOUS
Indicates that Dynamic Update type is continuous
|
static int |
_INCREMENTAL
Indicates that Dynamic Update type is incremental
|
static int |
_NONE
Indicates that Dynamic Update type is not selected
|
static SessionModeling.DynamicUpdateType |
CONTINUOUS
Indicates that Dynamic Update type is continuous
|
static SessionModeling.DynamicUpdateType |
INCREMENTAL
Indicates that Dynamic Update type is incremental
|
static SessionModeling.DynamicUpdateType |
NONE
Indicates that Dynamic Update type is not selected
|
Modifier and Type | Method and Description |
---|---|
static SessionModeling.DynamicUpdateType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionModeling.DynamicUpdateType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionModeling.DynamicUpdateType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SessionModeling.DynamicUpdateType NONE
public static final SessionModeling.DynamicUpdateType INCREMENTAL
public static final SessionModeling.DynamicUpdateType CONTINUOUS
public static final int _NONE
public static final int _INCREMENTAL
public static final int _CONTINUOUS
public static SessionModeling.DynamicUpdateType valueOf(int value)
public static SessionModeling.DynamicUpdateType valueOf(String name)
public static SessionModeling.DynamicUpdateType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.