public static class PartDrafting.WidthType extends Enum
Modifier and Type | Method and Description |
---|---|
static PartDrafting.WidthType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartDrafting.WidthType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartDrafting.WidthType[] |
values()
Returns an array that contains the values for this enum.
|
public static final PartDrafting.WidthType ORIGINAL
public static final PartDrafting.WidthType THIN
public static final PartDrafting.WidthType NORMAL
public static final PartDrafting.WidthType THICK
public static final PartDrafting.WidthType THICKNESS_ONE
public static final PartDrafting.WidthType THICKNESS_TWO
public static final PartDrafting.WidthType THICKNESS_THREE
public static final PartDrafting.WidthType THICKNESS_FOUR
public static final PartDrafting.WidthType THICKNESS_FIVE
public static final PartDrafting.WidthType THICKNESS_SIX
public static final PartDrafting.WidthType THICKNESS_SEVEN
public static final PartDrafting.WidthType THICKNESS_EIGHT
public static final PartDrafting.WidthType THICKNESS_NINE
public static final int _ORIGINAL
public static final int _THIN
public static final int _NORMAL
public static final int _THICK
public static final int _THICKNESS_ONE
public static final int _THICKNESS_TWO
public static final int _THICKNESS_THREE
public static final int _THICKNESS_FOUR
public static final int _THICKNESS_FIVE
public static final int _THICKNESS_SIX
public static final int _THICKNESS_SEVEN
public static final int _THICKNESS_EIGHT
public static final int _THICKNESS_NINE
public static PartDrafting.WidthType valueOf(int value)
public static PartDrafting.WidthType valueOf(String name)
public static PartDrafting.WidthType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.