Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SignalChartListItem.Condition |
SignalChartListItem.Condition.GREATER_THAN
Greater than
|
static SignalChartListItem.Condition |
SignalChartListItem.Condition.LESS_THAN
Less than
|
Modifier and Type | Method and Description |
---|---|
SignalChartListItem.Condition |
SignalChartListItem.eventCondition()
Returns the event condition
License requirements: nx_motion_motor ("NX Motion Motor") . |
static SignalChartListItem.Condition |
SignalChartListItem.Condition.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SignalChartListItem.Condition |
SignalChartListItem.Condition.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SignalChartListItem.Condition[] |
SignalChartListItem.Condition.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SignalChartListItem.setEventCondition(SignalChartListItem.Condition condition)
License requirements: nx_motion_motor ("NX Motion Motor") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.