Package | Description |
---|---|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
BodyContact
Represents a
BodyContact
To create or edit an instance of this class, use BodyContactBuilder Created in NX5.0.0 |
interface |
Bushing
Represents a bushing
To create or edit an instance of this class, use BushingBuilder Created in NX6.0.0 |
interface |
Connector
Represents a connector
This is an abstract class, and cannot be created. |
interface |
Coupler
Represents a motion coupler object
This is an abstract class, and cannot be created. |
interface |
CouplerCable
Represents a motion cable object
To create or edit an instance of this class, use CouplerCableBuilder Created in NX6.0.0 |
interface |
CouplerGear
Represents a motion gear object
To create or edit an instance of this class, use CouplerGearBuilder Created in NX6.0.0 |
interface |
CouplerRckpn
Represents a motion rack and pinion object
To create or edit an instance of this class, use CouplerRckpnBuilder Created in NX6.0.0 |
interface |
CurveContact
Represents a
CurveContact
To create or edit an instance of this class, use CurveContactBuilder Created in NX5.0.0 |
interface |
CurveOnCurve
Represents a curve on curve
To create or edit an instance of this class, use CurveOnCurveBuilder Created in NX6.0.0 |
interface |
Damper
Represents a damper
To create or edit an instance of this class, use DamperBuilder Created in NX6.0.0 |
interface |
FlexBody
Represents the Motion FlexBody class.It must be associated
with a Motion Link.
|
interface |
GeneralCoupler
Represents motion 2-3 joint coupler
To create or edit an instance of this class, use GeneralCouplerBuilder Created in NX7.5.0 |
interface |
Joint
Represents a motion joint object
To create or edit an instance of this class, use JointBuilder Created in NX5.0.0 |
interface |
Link
Represents the Motion Link class.
|
interface |
LoadTransfer
Represents a Motion Load Transfer class
To create or edit an instance of this class, use LoadTransferBuilder Created in NX9.0.0 |
interface |
MotionSensor
Represents a motion sensor
To create or edit an instance of this class, use MotionSensorBuilder Created in NX6.0.0 |
interface |
Motor
Represents a motion motor base object class
This is an abstract class, and cannot be created. |
interface |
PMDCMotor
Represents a motion pmdc motor object
To create or edit an instance of this class, use PMDCMotorBuilder Created in NX6.0.0 |
interface |
PointOnCurve
Represents a point on curve
To create or edit an instance of this class, use PointOnCurveBuilder Created in NX6.0.0 |
interface |
PointOnSurface
Represents a point on surface motion object
To create or edit an instance of this class, use PointOnSurfaceBuilder Created in NX6.0.0 |
interface |
ScalarForce
Represents the Motion ScalarForce class.
|
interface |
ScalarTorque
Represents the Motion ScalarTorque class.
|
interface |
Spring
Represents a spring
To create or edit an instance of this class, use SpringBuilder Created in NX6.0.0 |
interface |
VectorForce
Represents a vector force
To create or edit an instance of this class, use VectorForceBuilder Created in NX5.0.0 |
interface |
VectorTorque
Represents a vector torque
To create or edit an instance of this class, use VectorTorqueBuilder Created in NX5.0.0 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.