Package | Description |
---|---|
nxopen.menubar |
Provides classes and interfaces for the Menu Bar.
|
Modifier and Type | Field and Description |
---|---|
static ContextMenuEntry.Type |
ContextMenuEntry.Type.LABEL
A label often used to divide and provide context to sub-groups of commands.
|
static ContextMenuEntry.Type |
ContextMenuEntry.Type.PUSH_BUTTON
Has a command that is run when this entry is activated.
|
static ContextMenuEntry.Type |
ContextMenuEntry.Type.SEPARATOR
A visual divider between sections of the menu.
|
static ContextMenuEntry.Type |
ContextMenuEntry.Type.SUBMENU
Has an attached menu structure containing more entries.
|
static ContextMenuEntry.Type |
ContextMenuEntry.Type.TOGGLE_BUTTON
Displays an On/Off state.
|
Modifier and Type | Method and Description |
---|---|
ContextMenuEntry.Type |
ContextMenuEntry.entryType()
Returns the type of this menu entry.
|
static ContextMenuEntry.Type |
ContextMenuEntry.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ContextMenuEntry.Type |
ContextMenuEntry.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ContextMenuEntry.Type[] |
ContextMenuEntry.Type.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.