Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Field and Description |
---|---|
static RigidBodyBuilder.MassPropertiesOption |
RigidBodyBuilder.MassPropertiesOption.AUTOMATIC
automatic
|
static RigidBodyBuilder.MassPropertiesOption |
RigidBodyBuilder.MassPropertiesOption.USER_DEFINED
user defined
|
Modifier and Type | Method and Description |
---|---|
RigidBodyBuilder.MassPropertiesOption |
RigidBodyBuilder.massProperty()
Returns the auto-calculate mass property flag which is used to indicate whether all mass
properties are calculated by system.
|
static RigidBodyBuilder.MassPropertiesOption |
RigidBodyBuilder.MassPropertiesOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RigidBodyBuilder.MassPropertiesOption |
RigidBodyBuilder.MassPropertiesOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RigidBodyBuilder.MassPropertiesOption[] |
RigidBodyBuilder.MassPropertiesOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RigidBodyBuilder.setMassProperty(RigidBodyBuilder.MassPropertiesOption massProperty)
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.