Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Method and Description |
---|---|
ProxyObjectParameterBuilder |
ProxyOverrideObjectCollection.createProxyObjectParameterBuilder()
Creates a
ProxyObjectParameterBuilder
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") Created in NX8.5.0 |
ProxyObjectParameterBuilder |
ProxyObjectCollection.createProxyObjectParameterBuilder()
Creates a
ProxyObjectParameterBuilder
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") Created in NX8.5.0 |
ProxyObjectParameterBuilder |
ProxyObjectParameterBuilderList.findItem(int index)
Returns the object at the input index.
|
ProxyObjectParameterBuilder[] |
ProxyObjectParameterBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ProxyObjectParameterBuilderList.append(ProxyObjectParameterBuilder object)
Appends an object to the list
License requirements: None. |
void |
ProxyObjectParameterBuilderList.append(ProxyObjectParameterBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ProxyObjectParameterBuilderList.erase(ProxyObjectParameterBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
ProxyObjectParameterBuilderList.erase(ProxyObjectParameterBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ProxyObjectParameterBuilderList.findIndex(ProxyObjectParameterBuilder obj)
Finds the index where the input object appears.
|
void |
ProxyObjectParameterBuilderList.insert(int location,
ProxyObjectParameterBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
ProxyObjectParameterBuilderList.setContents(ProxyObjectParameterBuilder[] objects)
Sets the contents of the entire list.
|
void |
ProxyObjectParameterBuilderList.swap(ProxyObjectParameterBuilder object1,
ProxyObjectParameterBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.