Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Field and Description |
---|---|
static ComparisonResultElectricalPart.Status |
ComparisonResultElectricalPart.Status.ADDED
Added status
|
static ComparisonResultElectricalPart.Status |
ComparisonResultElectricalPart.Status.IDENTICAL
Identical status
|
static ComparisonResultElectricalPart.Status |
ComparisonResultElectricalPart.Status.REMOVED
Removed status
|
static ComparisonResultElectricalPart.Status |
ComparisonResultElectricalPart.Status.UPDATED
Updated status
|
Modifier and Type | Method and Description |
---|---|
ComparisonResultElectricalPart.Status |
ComparisonResultElectricalPart.comparisonStatus()
Returns the status from the electrical part
License requirements: None. |
static ComparisonResultElectricalPart.Status |
ComparisonResultElectricalPart.Status.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ComparisonResultElectricalPart.Status |
ComparisonResultElectricalPart.Status.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ComparisonResultElectricalPart.Status[] |
ComparisonResultElectricalPart.Status.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.