Package | Description |
---|---|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
Modifier and Type | Field and Description |
---|---|
static CamProfileBuilder.ProfileCyclicType |
CamProfileBuilder.ProfileCyclicType.CYCLIC
In Cyclic Cam Profiles the points at the beginning
and the end of the Master Axis range need to be identical
with respect to Slave Axis value, slope and curve.
|
static CamProfileBuilder.ProfileCyclicType |
CamProfileBuilder.ProfileCyclicType.NON_CYCLIC
Non-cyclic Cam Profiles are defined only in
the defined master axis range.
|
static CamProfileBuilder.ProfileCyclicType |
CamProfileBuilder.ProfileCyclicType.RELATIVE_CYCLIC
In Relative Cyclic Cam Profiles the start point and
end point of the profile do not necessarily have to be
equal.
|
Modifier and Type | Method and Description |
---|---|
CamProfileBuilder.ProfileCyclicType |
CamProfileBuilder.cyclicType()
Returns the cyclic type of a cam profile
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") . |
static CamProfileBuilder.ProfileCyclicType |
CamProfileBuilder.ProfileCyclicType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CamProfileBuilder.ProfileCyclicType |
CamProfileBuilder.ProfileCyclicType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CamProfileBuilder.ProfileCyclicType[] |
CamProfileBuilder.ProfileCyclicType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CamProfileBuilder.setCyclicType(CamProfileBuilder.ProfileCyclicType cyclicType)
License requirements: nx_mcd_core ("MECHATRONICS CONCEPT DESIGNER") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.