Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static TransitionCurveBuilder.TangentDirections |
TransitionCurveBuilder.TangentDirections.LIMIT
transition curve will be tangent to the limit curve
|
static TransitionCurveBuilder.TangentDirections |
TransitionCurveBuilder.TangentDirections.RAIL
transition curve will be tangent to the blend rail curve
|
Modifier and Type | Method and Description |
---|---|
TransitionCurveBuilder.TangentDirections |
TransitionCurveBuilder.endTangentDirection()
Returns the end tangent direction
License requirements: None. |
TransitionCurveBuilder.TangentDirections |
TransitionCurveBuilder.startTangentDirection()
Returns the start tangent direction
License requirements: None. |
static TransitionCurveBuilder.TangentDirections |
TransitionCurveBuilder.TangentDirections.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TransitionCurveBuilder.TangentDirections |
TransitionCurveBuilder.TangentDirections.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TransitionCurveBuilder.TangentDirections[] |
TransitionCurveBuilder.TangentDirections.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TransitionCurveBuilder.setEndTangentDirection(TransitionCurveBuilder.TangentDirections direction)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
TransitionCurveBuilder.setStartTangentDirection(TransitionCurveBuilder.TangentDirections direction)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.