Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
StyledSweepDoubleOnPathDimBuilder |
StyledSweepBuilder.createPivotSet(double value1,
double value2,
Curve path1,
Curve path2)
Creates a new pivot set
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Modifier and Type | Method and Description |
---|---|
StyledSweepDoubleOnPathDimBuilder |
StyledSweepDoubleOnPathDimBuilderList.findItem(int index)
Returns the object at the input index.
|
StyledSweepDoubleOnPathDimBuilder[] |
StyledSweepDoubleOnPathDimBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
StyledSweepDoubleOnPathDimBuilderList.append(StyledSweepDoubleOnPathDimBuilder object)
Appends an object to the list
License requirements: None. |
void |
StyledSweepDoubleOnPathDimBuilderList.append(StyledSweepDoubleOnPathDimBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
StyledSweepDoubleOnPathDimBuilderList.erase(StyledSweepDoubleOnPathDimBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
StyledSweepDoubleOnPathDimBuilderList.erase(StyledSweepDoubleOnPathDimBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
StyledSweepDoubleOnPathDimBuilderList.findIndex(StyledSweepDoubleOnPathDimBuilder obj)
Finds the index where the input object appears.
|
void |
StyledSweepDoubleOnPathDimBuilderList.insert(int location,
StyledSweepDoubleOnPathDimBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
StyledSweepDoubleOnPathDimBuilderList.setContents(StyledSweepDoubleOnPathDimBuilder[] objects)
Sets the contents of the entire list.
|
void |
StyledSweepDoubleOnPathDimBuilderList.swap(StyledSweepDoubleOnPathDimBuilder object1,
StyledSweepDoubleOnPathDimBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.