Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static SpiralPattern.SpiralDefineSize |
SpiralPattern.SpiralDefineSize.NUMBER_OF_TURNS
using number of turns to define size of spiral
|
static SpiralPattern.SpiralDefineSize |
SpiralPattern.SpiralDefineSize.TOTAL_ANGLE
using total angle to define size of spiral
|
Modifier and Type | Method and Description |
---|---|
SpiralPattern.SpiralDefineSize |
SpiralPattern.sizeSpiralType()
Returns the size spiral type
License requirements: None. |
static SpiralPattern.SpiralDefineSize |
SpiralPattern.SpiralDefineSize.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SpiralPattern.SpiralDefineSize |
SpiralPattern.SpiralDefineSize.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SpiralPattern.SpiralDefineSize[] |
SpiralPattern.SpiralDefineSize.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SpiralPattern.setSizeSpiralType(SpiralPattern.SpiralDefineSize sizeSpiralType)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.