Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static SelectDividingObjectBuilder.ToolType |
SelectDividingObjectBuilder.ToolType.ISOPARAMETRIC_CURVE |
static SelectDividingObjectBuilder.ToolType |
SelectDividingObjectBuilder.ToolType.LINE_BY_TWO_POINTS |
static SelectDividingObjectBuilder.ToolType |
SelectDividingObjectBuilder.ToolType.OBJECT |
static SelectDividingObjectBuilder.ToolType |
SelectDividingObjectBuilder.ToolType.OFFSET_CURVE_IN_FACE |
Modifier and Type | Method and Description |
---|---|
SelectDividingObjectBuilder.ToolType |
SelectDividingObjectBuilder.toolOption()
Returns the tool option
License requirements: None. |
static SelectDividingObjectBuilder.ToolType |
SelectDividingObjectBuilder.ToolType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SelectDividingObjectBuilder.ToolType |
SelectDividingObjectBuilder.ToolType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SelectDividingObjectBuilder.ToolType[] |
SelectDividingObjectBuilder.ToolType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SelectDividingObjectBuilder.setToolOption(SelectDividingObjectBuilder.ToolType toolOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.