Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
ScalingSetBuilder |
StyledSweepBuilder.createScalingSet(double valuePar,
double depthPar,
double pathPar,
Curve path)
Creates a new scaling set
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Modifier and Type | Method and Description |
---|---|
ScalingSetBuilder |
ScalingSetBuilderList.findItem(int index)
Returns the object at the input index.
|
ScalingSetBuilder[] |
ScalingSetBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ScalingSetBuilderList.append(ScalingSetBuilder object)
Appends an object to the list
License requirements: None. |
void |
ScalingSetBuilderList.append(ScalingSetBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ScalingSetBuilderList.erase(ScalingSetBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
ScalingSetBuilderList.erase(ScalingSetBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ScalingSetBuilderList.findIndex(ScalingSetBuilder obj)
Finds the index where the input object appears.
|
void |
ScalingSetBuilderList.insert(int location,
ScalingSetBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
ScalingSetBuilderList.setContents(ScalingSetBuilder[] objects)
Sets the contents of the entire list.
|
void |
ScalingSetBuilderList.swap(ScalingSetBuilder object1,
ScalingSetBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.