Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static RegionTracker.ExtremityType |
RegionTracker.ExtremityType.END
end
|
RegionTracker.ExtremityType[] |
RegionTracker.VertexSelectorsData.extremities
Extremity (false : start, true : end) of the edge corresponding to vertex
|
static RegionTracker.ExtremityType |
RegionTracker.ExtremityType.START
start
|
Modifier and Type | Method and Description |
---|---|
static RegionTracker.ExtremityType |
RegionTracker.ExtremityType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RegionTracker.ExtremityType |
RegionTracker.ExtremityType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RegionTracker.ExtremityType[] |
RegionTracker.ExtremityType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RegionTracker.setOneVertexSelector(Edge entity,
RegionTracker.ExtremityType extremity)
One input target or tool vertex (edge extremity) used to identify the region
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
RegionTracker.setVertexSelectors(Edge[] entities,
RegionTracker.ExtremityType[] extremities)
The input target or tool vertices (edge extremities) used to identify the region
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.