Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static ReduceSurfaceRadiusBuilder.ReducedFaceTypeSpecification |
ReduceSurfaceRadiusBuilder.ReducedFaceTypeSpecification.FACE_GROUP
Preview all items in face group list when using "Select Faces by Radius" to select input objects.
|
static ReduceSurfaceRadiusBuilder.ReducedFaceTypeSpecification |
ReduceSurfaceRadiusBuilder.ReducedFaceTypeSpecification.SINGLE_CHAIN
Preview single chain when using "Select Faces by Chain" and "Single Selection" to select input objects.
|
static ReduceSurfaceRadiusBuilder.ReducedFaceTypeSpecification |
ReduceSurfaceRadiusBuilder.ReducedFaceTypeSpecification.SINGLE_CHAIN_IN_GROUP
Preview single item in face group list when using "Select Faces by Radius" to select input objects.
|
Modifier and Type | Method and Description |
---|---|
ReduceSurfaceRadiusBuilder.ReducedFaceTypeSpecification |
ReduceSurfaceRadiusBuilder.reducedFaceType()
Returns the type of performing the radius reduction preview
License requirements: None. |
static ReduceSurfaceRadiusBuilder.ReducedFaceTypeSpecification |
ReduceSurfaceRadiusBuilder.ReducedFaceTypeSpecification.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ReduceSurfaceRadiusBuilder.ReducedFaceTypeSpecification |
ReduceSurfaceRadiusBuilder.ReducedFaceTypeSpecification.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ReduceSurfaceRadiusBuilder.ReducedFaceTypeSpecification[] |
ReduceSurfaceRadiusBuilder.ReducedFaceTypeSpecification.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ReduceSurfaceRadiusBuilder.setReducedFaceType(ReduceSurfaceRadiusBuilder.ReducedFaceTypeSpecification reducedFaceType)
License requirements: nx_freeform_2 ("advanced freeform modeling") OR die_engineering ("DIE ENGINEERING") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.