Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static Rebuild.DegreeTypes |
Rebuild.DegreeTypes.CUBIC
The rebuild degree is cubic.
|
static Rebuild.DegreeTypes |
Rebuild.DegreeTypes.QUINTIC
The rebuild degree is quintic
|
Modifier and Type | Method and Description |
---|---|
Rebuild.DegreeTypes |
Rebuild.degreeType()
Returns the degree type when rebuild type is none.
|
static Rebuild.DegreeTypes |
Rebuild.DegreeTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Rebuild.DegreeTypes |
Rebuild.DegreeTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Rebuild.DegreeTypes[] |
Rebuild.DegreeTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
Rebuild.setDegreeType(Rebuild.DegreeTypes degreeType)
Sets the degree type when rebuild type is none.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.