Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static ProjectionOptions.DirectionType |
ProjectionOptions.DirectionType.CRV_PLANE_NORMAL
Curve plane Normal
|
static ProjectionOptions.DirectionType |
ProjectionOptions.DirectionType.FACE_NORMAL
Face Normal
|
static ProjectionOptions.DirectionType |
ProjectionOptions.DirectionType.VECTOR
Vector Constructor
|
Modifier and Type | Method and Description |
---|---|
ProjectionOptions.DirectionType |
ProjectionOptions.projectDirectionMethod()
Returns the Projection direction method
License requirements: None. |
static ProjectionOptions.DirectionType |
ProjectionOptions.DirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ProjectionOptions.DirectionType |
ProjectionOptions.DirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ProjectionOptions.DirectionType[] |
ProjectionOptions.DirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ProjectionOptions.setProjectDirectionMethod(ProjectionOptions.DirectionType projectDirectionMethod)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.