Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static PolygonPattern.SizeOptions |
PolygonPattern.SizeOptions.CIRCUMSCRIBED
use circumscribed circle to define a polygon
|
static PolygonPattern.SizeOptions |
PolygonPattern.SizeOptions.INSCRIBED
use inscribed circle to define a polygon
|
Modifier and Type | Method and Description |
---|---|
PolygonPattern.SizeOptions |
PolygonPattern.polygonSizeOption()
Returns the polygon size option
License requirements: None. |
static PolygonPattern.SizeOptions |
PolygonPattern.SizeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PolygonPattern.SizeOptions |
PolygonPattern.SizeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PolygonPattern.SizeOptions[] |
PolygonPattern.SizeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PolygonPattern.setPolygonSizeOption(PolygonPattern.SizeOptions option)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.