Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static PointsFromFileBuilder.Options |
PointsFromFileBuilder.Options.ABSOLUTE
Absolute coordinates
|
static PointsFromFileBuilder.Options |
PointsFromFileBuilder.Options.WCS
Work coordinates
|
Modifier and Type | Method and Description |
---|---|
PointsFromFileBuilder.Options |
PointsFromFileBuilder.coordinateOption()
Returns the option indicating type of point coordinates
License requirements: None. |
static PointsFromFileBuilder.Options |
PointsFromFileBuilder.Options.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PointsFromFileBuilder.Options |
PointsFromFileBuilder.Options.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PointsFromFileBuilder.Options[] |
PointsFromFileBuilder.Options.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PointsFromFileBuilder.setCoordinateOption(PointsFromFileBuilder.Options option)
Sets the option indicating type of point coordinates
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.