Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static PatternFill.PatternFillOptions |
PatternFill.PatternFillOptions.EXCLUDE_AREA_ONLY
section is for exclude area only
|
static PatternFill.PatternFillOptions |
PatternFill.PatternFillOptions.FILLBY_BOUNDARY
section is for fill area.
|
static PatternFill.PatternFillOptions |
PatternFill.PatternFillOptions.FILLBY_FACE
section is face-based, and for fill area.
|
static PatternFill.PatternFillOptions |
PatternFill.PatternFillOptions.NONE
no section is defined
|
Modifier and Type | Method and Description |
---|---|
PatternFill.PatternFillOptions |
PatternFill.fillOptions()
Returns the fill options
License requirements: None. |
static PatternFill.PatternFillOptions |
PatternFill.PatternFillOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PatternFill.PatternFillOptions |
PatternFill.PatternFillOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PatternFill.PatternFillOptions[] |
PatternFill.PatternFillOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PatternFill.setFillOptions(PatternFill.PatternFillOptions fillOptions)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.