Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static PartModuleInputBuilder.ModifiableGeometryOptions |
PartModuleInputBuilder.ModifiableGeometryOptions.SELECTED
the faces/edges on shared body that are allowed for selection inside part module
|
static PartModuleInputBuilder.ModifiableGeometryOptions |
PartModuleInputBuilder.ModifiableGeometryOptions.WHOLE_BODY
the whole shared body will be allowed for selection inside part module
|
Modifier and Type | Method and Description |
---|---|
PartModuleInputBuilder.ModifiableGeometryOptions |
PartModuleInputBuilder.modifiableGeometryOption()
Returns the Modifiable Geometry option
License requirements: None. |
static PartModuleInputBuilder.ModifiableGeometryOptions |
PartModuleInputBuilder.ModifiableGeometryOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PartModuleInputBuilder.ModifiableGeometryOptions |
PartModuleInputBuilder.ModifiableGeometryOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PartModuleInputBuilder.ModifiableGeometryOptions[] |
PartModuleInputBuilder.ModifiableGeometryOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PartModuleInputBuilder.setModifiableGeometryOption(PartModuleInputBuilder.ModifiableGeometryOptions modifiableGeometryOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.