Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static MirrorPattern.PlaneOptions |
MirrorPattern.PlaneOptions.EXISTING
existing plane
|
static MirrorPattern.PlaneOptions |
MirrorPattern.PlaneOptions.NEW
new plane
|
Modifier and Type | Method and Description |
---|---|
MirrorPattern.PlaneOptions |
MirrorPattern.planeOption()
Returns the plane option
License requirements: None. |
static MirrorPattern.PlaneOptions |
MirrorPattern.PlaneOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorPattern.PlaneOptions |
MirrorPattern.PlaneOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorPattern.PlaneOptions[] |
MirrorPattern.PlaneOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MirrorPattern.setPlaneOption(MirrorPattern.PlaneOptions planeOptions)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.