Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
EntityUsageInfo |
EntityUsageInfoList.findItem(int index)
Returns the object at the input index.
|
EntityUsageInfo[] |
EntityUsageInfoList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
EntityUsageInfoList.append(EntityUsageInfo object)
Appends an object to the list
License requirements: None. |
void |
EntityUsageInfoList.append(EntityUsageInfo[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
EntityUsageInfoList.erase(EntityUsageInfo obj)
Erases the object from the list, but does not delete the object.
|
void |
EntityUsageInfoList.erase(EntityUsageInfo obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
EntityUsageInfoList.findIndex(EntityUsageInfo obj)
Finds the index where the input object appears.
|
void |
EntityUsageInfoList.insert(int location,
EntityUsageInfo object)
Inserts an object at the specified location
License requirements: None. |
void |
EntityUsageInfoList.setContents(EntityUsageInfo[] objects)
Sets the contents of the entire list.
|
void |
EntityUsageInfoList.swap(EntityUsageInfo object1,
EntityUsageInfo object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.