Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static CurveShapingBuilder.InsertionMethodOptions |
CurveShapingBuilder.InsertionMethodOptions.BETWEEN_POINTS
Insert points between points
|
static CurveShapingBuilder.InsertionMethodOptions |
CurveShapingBuilder.InsertionMethodOptions.THROUGH_POINTS
Insert points through points
|
static CurveShapingBuilder.InsertionMethodOptions |
CurveShapingBuilder.InsertionMethodOptions.UNIFORM
Insert points uniformly
|
Modifier and Type | Method and Description |
---|---|
CurveShapingBuilder.InsertionMethodOptions |
CurveShapingBuilder.insertionMethod()
Returns the point insertion method
License requirements: None. |
static CurveShapingBuilder.InsertionMethodOptions |
CurveShapingBuilder.InsertionMethodOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CurveShapingBuilder.InsertionMethodOptions |
CurveShapingBuilder.InsertionMethodOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CurveShapingBuilder.InsertionMethodOptions[] |
CurveShapingBuilder.InsertionMethodOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CurveShapingBuilder.setInsertionMethod(CurveShapingBuilder.InsertionMethodOptions insertionMethod)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.