Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static CurveFitOptions.FitMethod |
CurveFitOptions.FitMethod.ADVANCED
Advanced
|
static CurveFitOptions.FitMethod |
CurveFitOptions.FitMethod.CUBIC
Cubic
|
static CurveFitOptions.FitMethod |
CurveFitOptions.FitMethod.QUINTIC
Quintic
|
Modifier and Type | Method and Description |
---|---|
CurveFitOptions.FitMethod |
CurveFitOptions.fitOption()
Returns the curve fit method
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
static CurveFitOptions.FitMethod |
CurveFitOptions.FitMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CurveFitOptions.FitMethod |
CurveFitOptions.FitMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CurveFitOptions.FitMethod[] |
CurveFitOptions.FitMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CurveFitOptions.setFitOption(CurveFitOptions.FitMethod curveFitMethod)
Sets the curve fit method
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.