Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static BridgeCurveConnectivity.FaceDirectionOptions |
BridgeCurveConnectivity.FaceDirectionOptions.ISO_U
Along U iso-parameter
|
static BridgeCurveConnectivity.FaceDirectionOptions |
BridgeCurveConnectivity.FaceDirectionOptions.ISO_V
Along V iso-parameter
|
static BridgeCurveConnectivity.FaceDirectionOptions |
BridgeCurveConnectivity.FaceDirectionOptions.SECTIONAL
Sectional direction
|
Modifier and Type | Method and Description |
---|---|
BridgeCurveConnectivity.FaceDirectionOptions |
BridgeCurveConnectivity.faceDirectionOption()
Returns the face direction option
License requirements: None. |
static BridgeCurveConnectivity.FaceDirectionOptions |
BridgeCurveConnectivity.FaceDirectionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveConnectivity.FaceDirectionOptions |
BridgeCurveConnectivity.FaceDirectionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveConnectivity.FaceDirectionOptions[] |
BridgeCurveConnectivity.FaceDirectionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeCurveConnectivity.setFaceDirectionOption(BridgeCurveConnectivity.FaceDirectionOptions faceDirectionOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR nx_freeform_1 ("basic freeform modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.