Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static BridgeCurveConnectivity.CurveDirectionOptions |
BridgeCurveConnectivity.CurveDirectionOptions.PERPENDICULAR
Perpendicular to section using a reference face
|
static BridgeCurveConnectivity.CurveDirectionOptions |
BridgeCurveConnectivity.CurveDirectionOptions.TANGENT
Tangent to section
|
Modifier and Type | Method and Description |
---|---|
BridgeCurveConnectivity.CurveDirectionOptions |
BridgeCurveConnectivity.curveDirectionOption()
Returns the curve direction option
License requirements: None. |
static BridgeCurveConnectivity.CurveDirectionOptions |
BridgeCurveConnectivity.CurveDirectionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveConnectivity.CurveDirectionOptions |
BridgeCurveConnectivity.CurveDirectionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveConnectivity.CurveDirectionOptions[] |
BridgeCurveConnectivity.CurveDirectionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeCurveConnectivity.setCurveDirectionOption(BridgeCurveConnectivity.CurveDirectionOptions curveDirectionOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR nx_freeform_1 ("basic freeform modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.