Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static BoundingObjectBuilder.Method |
BoundingObjectBuilder.Method.BY_PLANE
By Plane
|
static BoundingObjectBuilder.Method |
BoundingObjectBuilder.Method.EXISTING_CURVE
Existing Curve
|
static BoundingObjectBuilder.Method |
BoundingObjectBuilder.Method.LINE_BY2POINTS
Line by 2 Points
|
static BoundingObjectBuilder.Method |
BoundingObjectBuilder.Method.POINT_AND_VECTOR
Point and Vector
|
static BoundingObjectBuilder.Method |
BoundingObjectBuilder.Method.PROJECT_POINT
Project Point
|
Modifier and Type | Method and Description |
---|---|
BoundingObjectBuilder.Method |
BoundingObjectBuilder.boundingObjectMethod()
Returns the bounding object method
License requirements: None. |
static BoundingObjectBuilder.Method |
BoundingObjectBuilder.Method.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BoundingObjectBuilder.Method |
BoundingObjectBuilder.Method.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BoundingObjectBuilder.Method[] |
BoundingObjectBuilder.Method.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BoundingObjectBuilder.setBoundingObjectMethod(BoundingObjectBuilder.Method boundingObjectMethod)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.