Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static BooleanToolBuilder.BooleanToolType |
BooleanToolBuilder.BooleanToolType.EXTRUDE
Tool consists of extrude created on the fly
|
static BooleanToolBuilder.BooleanToolType |
BooleanToolBuilder.BooleanToolType.FACE_OR_PLANE
Tool consists of sets of faces or datum planes
|
static BooleanToolBuilder.BooleanToolType |
BooleanToolBuilder.BooleanToolType.NEW_PLANE
Tool consists of plane created on the fly
|
static BooleanToolBuilder.BooleanToolType |
BooleanToolBuilder.BooleanToolType.REVOLVE
Tool consists of revolve created on the fly
|
Modifier and Type | Method and Description |
---|---|
BooleanToolBuilder.BooleanToolType |
BooleanToolBuilder.toolOption()
Returns the boolean tool option
License requirements: None. |
static BooleanToolBuilder.BooleanToolType |
BooleanToolBuilder.BooleanToolType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BooleanToolBuilder.BooleanToolType |
BooleanToolBuilder.BooleanToolType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BooleanToolBuilder.BooleanToolType[] |
BooleanToolBuilder.BooleanToolType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BooleanToolBuilder.setToolOption(BooleanToolBuilder.BooleanToolType toolOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.