Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
BlendStopshortBuilder |
EdgeBlendBuilder.getNewStopshortData(int ssIndex)
Get an edge blend stop short data for the index provided
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
int |
EdgeBlendBuilder.addNewStopshortData(BlendStopshortBuilder builder)
Add an edge blend stop short data for an edge in the edge blend
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
EdgeBlendBuilder.removeNewStopshortData(BlendStopshortBuilder builder)
Remove an edge blend stop short corresponding to a BlendStopshortBuilder
License requirements: solid_modeling ("SOLIDS MODELING") . |
Modifier and Type | Method and Description |
---|---|
BlendStopshortBuilder |
BlendStopshortBuilderCollection.create(BlendStopshortBuilder.Choices mChoice,
Expression mOnPathExp,
Edge mPath,
boolean mIsFlipped,
Point mThruPoint)
Creates an BlendStopshortBuilder.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.