public static class AlignmentMethodBuilder.Type extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ANGLE |
static int |
_ARC_LENGTH |
static int |
_DEVELOPABLE |
static int |
_DISTANCE |
static int |
_PARAMETER |
static int |
_POINTS |
static int |
_SEGMENTS |
static int |
_SPINE_CURVE |
static int |
_SPLINE_POINTS |
static AlignmentMethodBuilder.Type |
ANGLE |
static AlignmentMethodBuilder.Type |
ARC_LENGTH |
static AlignmentMethodBuilder.Type |
DEVELOPABLE |
static AlignmentMethodBuilder.Type |
DISTANCE |
static AlignmentMethodBuilder.Type |
PARAMETER |
static AlignmentMethodBuilder.Type |
POINTS |
static AlignmentMethodBuilder.Type |
SEGMENTS |
static AlignmentMethodBuilder.Type |
SPINE_CURVE |
static AlignmentMethodBuilder.Type |
SPLINE_POINTS |
Modifier and Type | Method and Description |
---|---|
static AlignmentMethodBuilder.Type |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AlignmentMethodBuilder.Type |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AlignmentMethodBuilder.Type[] |
values()
Returns an array that contains the values for this enum.
|
public static final AlignmentMethodBuilder.Type PARAMETER
public static final AlignmentMethodBuilder.Type ARC_LENGTH
public static final AlignmentMethodBuilder.Type POINTS
public static final AlignmentMethodBuilder.Type DISTANCE
public static final AlignmentMethodBuilder.Type ANGLE
public static final AlignmentMethodBuilder.Type SPINE_CURVE
public static final AlignmentMethodBuilder.Type SPLINE_POINTS
public static final AlignmentMethodBuilder.Type SEGMENTS
public static final AlignmentMethodBuilder.Type DEVELOPABLE
public static final int _PARAMETER
public static final int _ARC_LENGTH
public static final int _POINTS
public static final int _DISTANCE
public static final int _ANGLE
public static final int _SPINE_CURVE
public static final int _SPLINE_POINTS
public static final int _SEGMENTS
public static final int _DEVELOPABLE
public static AlignmentMethodBuilder.Type valueOf(int value)
public static AlignmentMethodBuilder.Type valueOf(String name)
public static AlignmentMethodBuilder.Type[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.