Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static MirrorCertificationBuilder.PassengerSideStandardsType |
MirrorCertificationBuilder.PassengerSideStandardsType.AUSTRALIA_ADR1402
Represents Australia : ADR 14/02 standard
|
static MirrorCertificationBuilder.PassengerSideStandardsType |
MirrorCertificationBuilder.PassengerSideStandardsType.CHINA_M1N1ONLY_GB150842006
Represents China (M1/N1 only) : GB 15084 - 2006 standard
|
static MirrorCertificationBuilder.PassengerSideStandardsType |
MirrorCertificationBuilder.PassengerSideStandardsType.CHINA_NOT_M1N1GB150842006
Represents China (Not M1/N1) : GB 15084 - 2006 standard
|
static MirrorCertificationBuilder.PassengerSideStandardsType |
MirrorCertificationBuilder.PassengerSideStandardsType.EUROPE_M1N1CLASSIII_MIRROR200397EC_ECER4602
Represents Europe (M1/N1_Class III Mirror) : 2003/97/EC - ECE R46.02 standard
|
static MirrorCertificationBuilder.PassengerSideStandardsType |
MirrorCertificationBuilder.PassengerSideStandardsType.EUROPE_M1N1ONLY71127EU_ECER4601SUPERCEDED
Represents Europe (M1/N1 only) : 71/127/EU - ECE R46.01 (Superceded ) standard
|
static MirrorCertificationBuilder.PassengerSideStandardsType |
MirrorCertificationBuilder.PassengerSideStandardsType.EUROPE_NOT_M1N171127EU_ECER4601SUPERCEDED
Represents Europe (Not M1/N1) : 71/127/EU - ECE R46.01 : (Superceded ) standard
|
static MirrorCertificationBuilder.PassengerSideStandardsType |
MirrorCertificationBuilder.PassengerSideStandardsType.JAPAN_ARTICLE44TRIAS29TRIAS39
Represents Japan : Article 44/TRIAS 29/TRIAS 39 standard
|
static MirrorCertificationBuilder.PassengerSideStandardsType |
MirrorCertificationBuilder.PassengerSideStandardsType.SAUDI_ARABIA_GULF_STATES_SSA770771GS421442
Represents Saudi Arabia - Gulf States : SSA 770/771 GS 421/442 standard
|
static MirrorCertificationBuilder.PassengerSideStandardsType |
MirrorCertificationBuilder.PassengerSideStandardsType.USA_CANADA_FMVSS111CMVSSS111
Represents USA - Canada : FMVSS111 - CMVSSS111 standard
|
Modifier and Type | Method and Description |
---|---|
MirrorCertificationBuilder.PassengerSideStandardsType |
MirrorCertificationBuilder.passengerSideStandard()
Returns the standard for passenger side mirror.
|
static MirrorCertificationBuilder.PassengerSideStandardsType |
MirrorCertificationBuilder.PassengerSideStandardsType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorCertificationBuilder.PassengerSideStandardsType |
MirrorCertificationBuilder.PassengerSideStandardsType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorCertificationBuilder.PassengerSideStandardsType[] |
MirrorCertificationBuilder.PassengerSideStandardsType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MirrorCertificationBuilder.setPassengerSideStandard(MirrorCertificationBuilder.PassengerSideStandardsType passengerSideStandard)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.