Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static MirrorCertificationBuilder.InstructionFieldPositionType |
MirrorCertificationBuilder.InstructionFieldPositionType.ON_ROAD_SURFACE
Represents that the instrucition field is on road surface
|
static MirrorCertificationBuilder.InstructionFieldPositionType |
MirrorCertificationBuilder.InstructionFieldPositionType.ON_TARGET_WALL
Represents that the instrucition field is on target wall
|
Modifier and Type | Method and Description |
---|---|
MirrorCertificationBuilder.InstructionFieldPositionType |
MirrorCertificationBuilder.instructionFieldPosition()
Returns the instruction field position, on wall or road.
|
static MirrorCertificationBuilder.InstructionFieldPositionType |
MirrorCertificationBuilder.InstructionFieldPositionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorCertificationBuilder.InstructionFieldPositionType |
MirrorCertificationBuilder.InstructionFieldPositionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorCertificationBuilder.InstructionFieldPositionType[] |
MirrorCertificationBuilder.InstructionFieldPositionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MirrorCertificationBuilder.setInstructionFieldPosition(MirrorCertificationBuilder.InstructionFieldPositionType instructionFieldPosition)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.