Package | Description |
---|---|
nxopen.features.subdivision |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static ExtractCagePolylineBuilder.InputCurveOption |
ExtractCagePolylineBuilder.InputCurveOption.DELETE
Delete input curves
|
static ExtractCagePolylineBuilder.InputCurveOption |
ExtractCagePolylineBuilder.InputCurveOption.HIDE
Hide input curves
|
static ExtractCagePolylineBuilder.InputCurveOption |
ExtractCagePolylineBuilder.InputCurveOption.KEEP
Keep input curves as they are
|
Modifier and Type | Method and Description |
---|---|
ExtractCagePolylineBuilder.InputCurveOption |
ExtractCagePolylineBuilder.inputCurveOptions()
Returns the input curve options
License requirements: None. |
static ExtractCagePolylineBuilder.InputCurveOption |
ExtractCagePolylineBuilder.InputCurveOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtractCagePolylineBuilder.InputCurveOption |
ExtractCagePolylineBuilder.InputCurveOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtractCagePolylineBuilder.InputCurveOption[] |
ExtractCagePolylineBuilder.InputCurveOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ExtractCagePolylineBuilder.setInputCurveOptions(ExtractCagePolylineBuilder.InputCurveOption inputCurveOptions)
License requirements: nx_subdivision (" NX SUBDIVISION") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.