Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static TrimExtendBuilder.ArrowSideOptions |
TrimExtendBuilder.ArrowSideOptions.DELETE
Delete
|
static TrimExtendBuilder.ArrowSideOptions |
TrimExtendBuilder.ArrowSideOptions.RETAIN
Retain
|
Modifier and Type | Method and Description |
---|---|
TrimExtendBuilder.ArrowSideOptions |
TrimExtendBuilder.arrowSideOption()
Returns the trim and extend arrow side option to specify to retain or discard material in trim operations when Limits are set to Until Selected
License requirements: None. |
static TrimExtendBuilder.ArrowSideOptions |
TrimExtendBuilder.ArrowSideOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimExtendBuilder.ArrowSideOptions |
TrimExtendBuilder.ArrowSideOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimExtendBuilder.ArrowSideOptions[] |
TrimExtendBuilder.ArrowSideOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimExtendBuilder.setArrowSideOption(TrimExtendBuilder.ArrowSideOptions arrowSideOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.