Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static TrimCurveBuilder.FirstBoundingObjectEndOptions |
TrimCurveBuilder.FirstBoundingObjectEndOptions.END
Trim first bounding object from end
|
static TrimCurveBuilder.FirstBoundingObjectEndOptions |
TrimCurveBuilder.FirstBoundingObjectEndOptions.START
Trim first bounding object from start
|
Modifier and Type | Method and Description |
---|---|
TrimCurveBuilder.FirstBoundingObjectEndOptions |
TrimCurveBuilder.firstBoundingObjectEndOption()
Returns the end of the first bounding object which would be trimmed
License requirements: None. |
static TrimCurveBuilder.FirstBoundingObjectEndOptions |
TrimCurveBuilder.FirstBoundingObjectEndOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimCurveBuilder.FirstBoundingObjectEndOptions |
TrimCurveBuilder.FirstBoundingObjectEndOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimCurveBuilder.FirstBoundingObjectEndOptions[] |
TrimCurveBuilder.FirstBoundingObjectEndOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimCurveBuilder.setFirstBoundingObjectEndOption(TrimCurveBuilder.FirstBoundingObjectEndOptions firstBoundingObjectEndOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.