Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionSurfaceBuilder.SectionMethodRhoEnum |
SectionSurfaceBuilder.SectionMethodRhoEnum.LEAST_TENSION
least tension method
|
static SectionSurfaceBuilder.SectionMethodRhoEnum |
SectionSurfaceBuilder.SectionMethodRhoEnum.RHO
rho law method
|
Modifier and Type | Method and Description |
---|---|
SectionSurfaceBuilder.SectionMethodRhoEnum |
SectionSurfaceBuilder.sectionMethodRho()
Deprecated.
Deprecated in NX9.0.0. Use
SectionSurfaceBuilderEx instead.
|
static SectionSurfaceBuilder.SectionMethodRhoEnum |
SectionSurfaceBuilder.SectionMethodRhoEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionSurfaceBuilder.SectionMethodRhoEnum |
SectionSurfaceBuilder.SectionMethodRhoEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionSurfaceBuilder.SectionMethodRhoEnum[] |
SectionSurfaceBuilder.SectionMethodRhoEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionSurfaceBuilder.setSectionMethodRho(SectionSurfaceBuilder.SectionMethodRhoEnum sectionMethodRho)
Deprecated.
Deprecated in NX9.0.0. Use
SectionSurfaceBuilderEx instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.