Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionInertiaAnalysisBuilder.SectionAxisNormal |
SectionInertiaAnalysisBuilder.SectionAxisNormal.XC
Along X Axis
|
static SectionInertiaAnalysisBuilder.SectionAxisNormal |
SectionInertiaAnalysisBuilder.SectionAxisNormal.YC
Along Y Axis
|
static SectionInertiaAnalysisBuilder.SectionAxisNormal |
SectionInertiaAnalysisBuilder.SectionAxisNormal.ZC
Along Z Axis
|
Modifier and Type | Method and Description |
---|---|
SectionInertiaAnalysisBuilder.SectionAxisNormal |
SectionInertiaAnalysisBuilder.sectionNormal()
Returns the section normal
License requirements: None. |
static SectionInertiaAnalysisBuilder.SectionAxisNormal |
SectionInertiaAnalysisBuilder.SectionAxisNormal.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionInertiaAnalysisBuilder.SectionAxisNormal |
SectionInertiaAnalysisBuilder.SectionAxisNormal.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionInertiaAnalysisBuilder.SectionAxisNormal[] |
SectionInertiaAnalysisBuilder.SectionAxisNormal.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionInertiaAnalysisBuilder.setSectionNormal(SectionInertiaAnalysisBuilder.SectionAxisNormal sectionNormal)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.