Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static RPOBuilder.AssociativityType |
RPOBuilder.AssociativityType.ARC_CENTER
Arc-center
|
static RPOBuilder.AssociativityType |
RPOBuilder.AssociativityType.END_POINT
End-point (determined from 3d help point)
|
static RPOBuilder.AssociativityType |
RPOBuilder.AssociativityType.END_POINT1
1st end point (at minimum parameter value)
|
static RPOBuilder.AssociativityType |
RPOBuilder.AssociativityType.END_POINT2
2nd end point
|
static RPOBuilder.AssociativityType |
RPOBuilder.AssociativityType.HORIZONTAL_CENTERLINE1
horizontal centerline end point 1
|
static RPOBuilder.AssociativityType |
RPOBuilder.AssociativityType.HORIZONTAL_CENTERLINE2
horizontal centerline end point 2
|
static RPOBuilder.AssociativityType |
RPOBuilder.AssociativityType.TANGENCY
Tangency
|
static RPOBuilder.AssociativityType |
RPOBuilder.AssociativityType.VERTICAL_CENTERLINE1
vertical centerline end point 1
|
static RPOBuilder.AssociativityType |
RPOBuilder.AssociativityType.VERTICAL_CENTERLINE2
vertical centerline end point 2
|
Modifier and Type | Method and Description |
---|---|
static RPOBuilder.AssociativityType |
RPOBuilder.AssociativityType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RPOBuilder.AssociativityType |
RPOBuilder.AssociativityType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RPOBuilder.AssociativityType[] |
RPOBuilder.AssociativityType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RPOBuilder.setTargetAndTool(PositioningDimension.Subtype subtype,
NXObject target,
RPOBuilder.AssociativityType targetAssociativity,
Point3d targetHelpPoint,
NXObject tool,
RPOBuilder.AssociativityType toolAssociativity,
Point3d toolHelpPoint)
Sets the target and tool entities.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.