Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MeshTransformerBuilder.MeshTopologyType |
MeshTransformerBuilder.MeshTopologyType.ALIGNED
Aligned
|
static MeshTransformerBuilder.MeshTopologyType |
MeshTransformerBuilder.MeshTopologyType.END_ONLY
End only
|
static MeshTransformerBuilder.MeshTopologyType |
MeshTransformerBuilder.MeshTopologyType.UNALIGNED
Unaligned
|
Modifier and Type | Method and Description |
---|---|
MeshTransformerBuilder.MeshTopologyType |
MeshTransformerBuilder.meshTopologyOption()
Returns the option for setting the mesh topology used in the transformation or morphing calculations
License requirements: None. |
static MeshTransformerBuilder.MeshTopologyType |
MeshTransformerBuilder.MeshTopologyType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MeshTransformerBuilder.MeshTopologyType |
MeshTransformerBuilder.MeshTopologyType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MeshTransformerBuilder.MeshTopologyType[] |
MeshTransformerBuilder.MeshTopologyType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MeshTransformerBuilder.setMeshTopologyOption(MeshTransformerBuilder.MeshTopologyType meshTopologyOption)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.