Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GuidedExtensionBuilderEx.SegmentType |
GuidedExtensionBuilderEx.SegmentType.BYPASS
Bypass segment type
|
static GuidedExtensionBuilderEx.SegmentType |
GuidedExtensionBuilderEx.SegmentType.NORMAL
Normal segment type
|
static GuidedExtensionBuilderEx.SegmentType |
GuidedExtensionBuilderEx.SegmentType.TRANSITION
Transition segment type
|
Modifier and Type | Method and Description |
---|---|
static GuidedExtensionBuilderEx.SegmentType |
GuidedExtensionBuilderEx.SegmentType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GuidedExtensionBuilderEx.SegmentType |
GuidedExtensionBuilderEx.SegmentType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GuidedExtensionBuilderEx.SegmentType[] |
GuidedExtensionBuilderEx.SegmentType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GuidedExtensionBuilderEx.setSelectedSegmentType(GuidedExtensionBuilderEx.SegmentType segmentType)
Sets the segment type for the selected segment.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.