Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GeomcopyBuilder.TransformTypes |
GeomcopyBuilder.TransformTypes.ALONG_CURVE
along a path
|
static GeomcopyBuilder.TransformTypes |
GeomcopyBuilder.TransformTypes.BETWEEN_LOCATIONS
between two point or csys locations
|
static GeomcopyBuilder.TransformTypes |
GeomcopyBuilder.TransformTypes.MIRROR
mirror about a plane
|
static GeomcopyBuilder.TransformTypes |
GeomcopyBuilder.TransformTypes.OFFSET
offset
|
static GeomcopyBuilder.TransformTypes |
GeomcopyBuilder.TransformTypes.ROTATION
rotation about an axis
|
static GeomcopyBuilder.TransformTypes |
GeomcopyBuilder.TransformTypes.TRANSLATION
translation along a direction
|
Modifier and Type | Method and Description |
---|---|
GeomcopyBuilder.TransformTypes |
GeomcopyBuilder.type()
Returns the transformation type of instancing, such as Between Locations, or Mirror.
|
static GeomcopyBuilder.TransformTypes |
GeomcopyBuilder.TransformTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeomcopyBuilder.TransformTypes |
GeomcopyBuilder.TransformTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeomcopyBuilder.TransformTypes[] |
GeomcopyBuilder.TransformTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GeomcopyBuilder.setType(GeomcopyBuilder.TransformTypes transformType)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.